TOLL FREE 800 774 3539

FAX 973 660 9330

alter Browser Firefox Browser Internet Explorer Browser Safari Browser Opera Browser
 
 

Cable & Wire Technical Characteristics

Q: When is an ÖLFLEX® or UNITRONIC® cable deemed "low-capacitance" and what advantages does this offer over other cables?
Q: Why do all connection and control cables feature two rated voltage ranges, for example U0/U 300/500 V?
Q: How do you convert the alternating current voltage value (AC) of an ÖLFLEX® cable into the corresponding direct current voltage value (DC)?
Q: Why can a cable not be loaded with the same current amperage when used in different ambient temperatures?
Q: Can the steel wire armour of the ÖLFLEX® CLASSIC 100 SY also be used as EMC-compliant electromagnetic shielding resp. screening?
Q: How do I obtain the capacitance, inductance and impedance values of ÖLFLEX® cables?
Q: What do I do if a customer requests the ampacity of an ÖLFLEX® cable and queries the ideal conductor cross-section for his application?
Q: Can a UNITRONIC® data cable with a peak operating voltage of 250 V be used to connect a device with a mains voltage of 230 V?
Q: Is it possible to load a cable or wire with a voltage class of 300/500 V with a higher voltage for a brief period, provided that the testing voltage value is not exceeded?
Q: What is the difference between a copper braid screening and an aluminum laminated foil screening?
Q: What does PUR, TPE, PVC & LSZH stand for?
Q: What stationary PVC or PUR control cables do we offer with color codes?
Q: What does OR-04 mean?
Q: What are the differences between ÖLFLEX Control TM and ÖLFLEX Tray II?
Q: What does CY, SY and CP mean?
Q: What does MTW mean and what is the intended application?
Q: When is an ÖLFLEX® or UNITRONIC® cable deemed "low-capacitance" and what advantages does this offer over other cables?
Q: Why do all connection and control cables feature two rated voltage ranges, for example U0/U 300/500 V?
Q: How do you convert the alternating current voltage value (AC) of an ÖLFLEX® cable into the corresponding direct current voltage value (DC)?
Q: Why can a cable not be loaded with the same current amperage when used in different ambient temperatures?
Q: Can the steel wire armor of the ÖLFLEX® CLASSIC 100 SY also be used as EMC-compliant electromagnetic shielding resp. screening?
Q: How do I obtain the capacitance, inductance and impedance values of ÖLFLEX® cables?
Q: What do I do if a customer requests the ampacity of an ÖLFLEX® cable and queries the ideal conductor cross-section for his application?
Q: Can a UNITRONIC® data cable with a peak operating voltage of 250 V be used to connect a device with a mains voltage of 230 V?
Q: Is it possible to load a cable or wire with a voltage class of 300/500 V with a higher voltage for a brief period, provided that the testing voltage value is not exceeded?
Q: What is the difference between a copper braid screening and an aluminum laminated foil screening?

Locate your Dealer

To find a Lapp Authorized Distributor nearest you, simply type your zip code or city and select from the list:

Corporate News